Technical FAQs

Ask a Question

What is the drop out point of the undervoltage trip device for the Powerpact H and J breakers??

The UVR devices drop out between 35% to 70% of rated voltage.


CTA-ID : 2053178
Was this helpful?
What can we do to improve the information ?