Technical FAQs

Ask a Question

What is the part number for the IP54 circuit breaker sealing boot for the Power Bus FA type circuit breaker plug-in unit?

The catalog number for the sealing boot is PBP54100FA. It is an IP 54 rated kit for the FA breaker.

CTA-ID : 2053139
Was this helpful?
What can we do to improve the information ?