Technical FAQs

Ask a Question

Can the MiniBreak switch be locked closed? The switch is in a public area and the customer does not want someone to open the switch.

MiniBreak is designed for lock open only. The customer can drill out the handle to be able to lock the switch closed. The exception to this where the switch is used as the Service Entrance disconnect switch. This should never be locked closed.


CTA-ID : 2053553
Was this helpful?
What can we do to improve the information ?