Technical FAQs

Ask a Question

What is the part number for an end closure for Type 1 and Type 2 underfloor duct?

A DBDP is used as an end closure for all of the different widths of duct. The DBDP is perforated to allow small sections to be broken off and used for the smaller duct.
DBDP IS OBSOLETE.



CTA-ID : 2053529
Was this helpful?
What can we do to improve the information ?