Technical FAQs

Ask a Question

Is it possible to adjust the fuse spacing in an QMJ365 fusible switch to accomodate different 400A fuse bodies?

The fuse clips in the QMJ365 are not adjustable, they must use a standard 400A Class J fuse size. However, it is possible to install fuses with different amperage elements, as long as the physical size of the fuse remains the same.

CTA-ID : 2053544
Was this helpful?
What can we do to improve the information ?