Technical FAQs

Ask a Question

Is the dissipated Watts Loss provided for CT / VT drives for Type 1 and Type 12/12K enclosures would be a linear number or not? i.e. If it`s at Full Load and Full Speed, would it be 1/2 the number given at 30 Hz under 1/2 load?

There are some losses that are constant for running the electronics, but this is small compared to the other losses. Between no load and load the losses will be a linear function of the current.


CTA-ID : 2053226
Was this helpful?
What can we do to improve the information ?