Technical FAQs

Ask a Question

Is the connector with screw terminals for the P frame motor operator replaceable?

The connector is installed as part of the electrically operated mechanism and does not come with replacement motors or coils. The connector assembly is not available as a replacement part.


CTA-ID : 2053500
Was this helpful?
What can we do to improve the information ?