Technical FAQs

Ask a Question

What the handle length for a GS1TU3, 800 amp disconnect? What is the orientation of the handle for the On position and Off position?

Handle is 7.5 inches long from the center line of the shaft to the end . Imagine a clock dial, the On position is at 6 O`clock, Off is at 3 O`clock.

CTA-ID : 2053749
Was this helpful?
What can we do to improve the information ?