Technical FAQs

Ask a Question

Customer has an HVL/cc switch. He is getting some strange readings on it and needs some troubleshooting help. What is acceptable for contact resistance of the switch itself?

Left vmail with Don Bedwell-Tag 11:19 CST
3/18 Emailed and assigned case to Don Bedwell. The contact resistance value should not exceed 300% of 80 micro-ohms using a 100A test micrometer. (240 micro-ohms maximum.

CTA-ID : 2053737
Was this helpful?
What can we do to improve the information ?