Technical FAQs

Ask a Question

Is there a door lock kit available for a QO612L100DSCU load center?

Yes, use PK8FL. However, this is only applicable to a Series G04 load center. Design Series earlier than Series G04 did not have a door lock kit available. The design Series Number can be found on the directory label located inside the door.

CTA-ID : 2053477
Was this helpful?
What can we do to improve the information ?