Technical FAQs

Ask a Question

What Type D pistol handles are available for the LK3DU3, IEC Disconnect Switch?

GS1AH101 for a black handle that is padlockable, rated IP54, Off/On operation.
GS1AH102 for a red/yellow handle that is padlockable, rated IP54, Off/On operation.


CTA-ID : 2053739
Was this helpful?
What can we do to improve the information ?