Technical FAQs

Ask a Question

Is the back panel of a 8539SDW43 combination starter also made of stainless steel?

No, only the enclosure is 304 Stainless.


CTA-ID : 2053702
Was this helpful?
What can we do to improve the information ?