Technical FAQs

Ask a Question

What is the purpose of the DSC1 coupler?

It supports the underfloor duct in its proper horizontal and vertical position during the concrete pour and also joins the lengths of duct.
PART NUMBER DSC1 IS NOW OBSOLETE.



CTA-ID : 2053517
Was this helpful?
What can we do to improve the information ?