Technical FAQs

Ask a Question

Does catalog number G2BAS2 does this come with the inserts? What is the catalog number of the closing cap?

The GB2BAS2 comes with both elliptical round adapters. The customer can choose which one he or she uses. Also. catalog number G153A is the closing cap. GB2BAS2 AND G153A ARE NOW OBSOLETE.


CTA-ID : 2053514
Was this helpful?
What can we do to improve the information ?