Technical FAQs

Ask a Question

Are the QOT tandem circuit breakers suitable for use with 2 wires?

No. The QOT circuit breakers have a box type lug suitable for one #14-#8 AWG copper or aluminum wire.


CTA-ID : 2053452
Was this helpful?
What can we do to improve the information ?