Technical FAQs

Ask a Question

Can the QOB315GFI, QOB315EPD or QOB315EPE branch breakers be used in a QON3B or QON3BRT OEM mounting base?

Issue:
Product design feature

Product line:
QO OEM Mounting Bases

Environment:
Branch breakers

Cause:
Application

Resolution:

Yes, but only in current design Series 2(or 002), available in February, 2010. The Series number can be identified on the package label or the devices wiring diagram. These breakers should not be used in any device with earlier Series numbers.


CTA-ID : 2053377
Was this helpful?
What can we do to improve the information ?