Technical FAQs

Ask a Question

Can a QO315GFI, QO315EPD or QO315EPE be used in a QO403L60NF Load Center?

Yes, but only in current design Series 003, available in February, 2010. The Series number can be identified on the package label or the devices wiring diagram. These breakers should not be used in any device with earlier Series numbers.

CTA-ID : 2053373
Was this helpful?
What can we do to improve the information ?