Technical FAQs

Ask a Question

What type of base does the 9001 Type O - 120v replacement lamp - 2550105005 have?<br /><br />What is the wattage and length of a 9001OR120? <br /><br />Is this a fairly bright lamp, it`s being used for security issue?

This uses Sylvania 120PSB lamp which is a 3 watt (.025 AMP) 120 volt T2 bulb shape, Type 5 Slide Base .

Overall length is 1.84` long.

Lumin output is .046

CTA-ID : 2053300
Was this helpful?
What can we do to improve the information ?