Technical FAQs

Ask a Question

9999SC9: What components are included with this kit?

Product Line:
 
Type S Accessories and Components

Resolution:
The parts included for the 9999 Type SC9 `Hand-Off-Auto` Selector Switch Kit are as follows:
Qty 1 - 9001 KA1 - Contact block.
Qty 1 - 9001 SKS43B - 3 position selector switch (no spring return).
Qty 1 - 9001 KN260BP - `HAND - OFF - AUTO` legend plate.
A wiring harness and instruction sheet are also included.


Used on ALL 8538, 8539 NEMA 4, 4X Combination Starters
Used on ALL 8538, 8539 NEMA 4, 4X Oversized `S8` Combination Starters




CTA-ID : 2053501
Was this helpful?
What can we do to improve the information ?