Technical FAQs

Ask a Question

<br /><br />What is the contact block replacement for a XY2CE switch?<br /><br />

The XESP2151 is a snap action block, 1-NO and 1-NC contact for the XY2CE and XY2CH normal action momentary contact cable pulls switches only. This contact block is not replaceable in the Emergency Stop circuits which use Slow make, Slow break contact blocks.

CTA-ID : 2053793
Was this helpful?
What can we do to improve the information ?