Technical FAQs

Ask a Question

What is the part number for an abandon outlet plate for the rectangular E type inserts used on the Subway underfloor duct?


Product Line:
Wire Management

NFPA 70 Art.354, Art. 356; UL884; UL209

Unused underfloor duct outlets must be properly closed.  Schneider Electric exited the underfloor duct business in 2007.

When they were available, either DSAOPA for Aluminum or DSAOPB for bronze were used to close abandoned outlets.  As these are obsolete and no longer available, with no substitutions, consider a similar product from a manufacturer still in the underfloor duct business, for example, Wiremold, as a substitution.

CTA-ID : 2053527
Was this helpful?
What can we do to improve the information ?