Technical FAQs

Ask a Question

What is the catalog number to get inserts spaced on 12 inch centers on the Subway Underfloor Duct?

Issue:
Selection

Product Line:
Wire Management

Environment:
NFPA 70 Art.354, Art. 356; UL884; UL209

Cause:
Changes to usage of a space can drive the need to modify existing underfloor duct installations.

Resolution:
The underfloor duct and its associated service fittings and accessories are now obsolete and no longer available.

Adding C12 to the end of the underfloor duct catalog number (ex DM1E10C12) designated inserts on 12 inch centers.




CTA-ID : 2053524
Was this helpful?
What can we do to improve the information ?