Technical FAQs

Ask a Question

Replacement NEMA 3R door for an MH**WP panelboard enclosure.

Issue:
Is there a replacement NEMA 3R door for an MH**WP panelboard enclosure?

Product Line:
PTFDS - FD Enclosure Systems

Environment:
Panelboard enclosures sold and supported in the USA.

Cause:
Can the door be replaced on a weatherproof Nema 3R/12 panelboard enclosure?

Resolution:
Replacement door kits are not available for NEMA 3R enclosures. The customer will be required to re-order an MH26WP.





















CTA-ID : 2053276
Was this helpful?
What can we do to improve the information ?