Technical FAQs

Ask a Question

Do the SG series magnetic sensors such as a catalog number SGC8025 come with the magnet?

No. SCG8025, for example, is the sensor part number alone. The magnets are sold separately and can be found on page 296 of catalog 9006CT0101which can be accessed on Technical Library or Google.


CTA-ID : 2053350
Was this helpful?
What can we do to improve the information ?