Technical FAQs

Ask a Question

What is the temperature rating for the cables attached to medium voltage switchgear?

Cables connected to all of our medium voltage switchgear should be rated 90 degrees Centigrade. Cables with a higher insulation temperature values should be treated as though they were 90 degree C rated.


CTA-ID : 2053071
Was this helpful?
What can we do to improve the information ?