Technical FAQs

Ask a Question

What is the horse power rating for a 82343 double throw transfer switch ?

The 82343 is rated 15 HP up to 600VAC.


CTA-ID : 2053039
Was this helpful?
What can we do to improve the information ?