Technical FAQs

Ask a Question

Are there clips or accessories needed to mount the 5 foot long RWTP60 divider in the wall duct?

Holes are provided to mount the partition into the duct, forming a 3.41 inch (87 mm) high divider. Mounting hardare is not included.

CTA-ID : 2053038
Was this helpful?
What can we do to improve the information ?