Technical FAQs

Ask a Question

What is the suffix 1486 on an FAL340801486?

1486 is for 2A and 2B auxiliary contacts in the right hand side and a 24V DC shunt trip on the left hand side. The breaker is also calibrated for 50 degree C ambient temperature.


CTA-ID : 2052996
Was this helpful?
What can we do to improve the information ?