Technical FAQs

Ask a Question

Is an 8940 pump panel available in a NEMA 12 enclosure?

No. The 8940 pump panels are only available in NEMA 3R enclosures. They are designed for use outdoors at remote wells.


CTA-ID : 2053283
Was this helpful?
What can we do to improve the information ?