Technical FAQs

Ask a Question

What is the NEMA rating for GV7AP01 rotary handle?

It does not have a NEMA rating it has an IP54 rating. It is suitable for use in a NEMA1 environment.


CTA-ID : 2053158
Was this helpful?
What can we do to improve the information ?