Technical FAQs

Ask a Question

Does Schneider Electric / Square D offer a 400 ampere load center in a NEMA Type 3R enclosure?

Issue:
Selection

Product Line:
Load Center

Cause:
Selection

Resolution:
Square D does offer a 400 ampere load center, but only in a NEMA Type 1 enclosure. For a NEMA Type 3R application, consider using a NQ panelboard.


CTA-ID : 2053034
Was this helpful?
What can we do to improve the information ?