Technical FAQs

Ask a Question

Can you have an integrally factory installed 225A internal lighting contactor in a NF430L4C panelboard with a Nema 4 enclosure? Or an I-LINE panelboard with a Nema 4 enclosure? EQM Product selectors won`t allow a selection

Issue:
Can you have an integrally factory installed  225A internal lighting contactor in a  NF430L4C panelboard with a Nema 4 enclosure? Or an  I-LINE panelboard with a Nema 4 enclosure? EQM Product selectors won`t allow a selection 

Product Line:
Panelboards.

Environment:
Products sold in the United States.

Cause:
Selection.

Resolution:
No, The NF panelboards with 400 amp bussing , does not have a intergral mounted Contactor, a separate, enclosed Contactor will need to be ordered. The I Line Panelboard will not accept this feature as welll, due to heat rise restrictions.


CTA-ID : 2053205
Was this helpful?
What can we do to improve the information ?