Technical FAQs

Ask a Question

Are the Multi 9 Lateral Rotary Handles suitable for installation on a NEMA 4 enclosure? Does it have a gasket to seal the shaft?

The Multi 9 Rotary Handles have an IEC IP 54 rating. IP54 is defined as being protected against water spray in all directions.
These include the MG27046 operating subassembly and the MG27047 drawout handle or the MG27048 fixed front or lateral handle.
The kit does not provide a gasket between the handle housing and the panel on which it is mounted. However, the through-hole is about 1-1/2 inches and the housing is about 3-1/3 inches diameter.


CTA-ID : 2053449
Was this helpful?
What can we do to improve the information ?