Technical FAQs

Ask a Question

HOMELINE and QO load centers have 1/4`` Knockouts or holes in the ends of the load center, and the customer wants to know what the knockouts are for?

These smaller knockouts are used for entry of the service grounding electrode conductor.


CTA-ID : 2053200
Was this helpful?
What can we do to improve the information ?