Technical FAQs

Ask a Question

What is the NEMA rating for GV2AP01 rotary handle?

It does not have a NEMA rating but it does have an IP54 rating. It is suitable for use in a NEMA 1 environment.


CTA-ID : 2053154
Was this helpful?
What can we do to improve the information ?