Technical FAQs

Ask a Question

On plug in adjustable timers such as a 9050JCK59V20 what does each line represent on the range setting? Is each marked line a percentage of the time setting?

The printed lines adjacent to the control knob on top of the timer do not represent actual time values. They are a reference scale for comparison of time settings only.


CTA-ID : 2053701
Was this helpful?
What can we do to improve the information ?