Technical FAQs

Ask a Question

Is keyed operation available in the 2, 3, and 4 position 30 MM selector switches in corrosion resistant construction?

No the 30 mm 9001SKS corrosion resistant operators do not have a keyed option. Customers must select the 9001KS non corrosion resistant type to obtain keyed operation.


CTA-ID : 2053239
Was this helpful?
What can we do to improve the information ?