Technical FAQs

Ask a Question

What are the percentages the voltages can be bucked or boosted using a buck boost transformer?

We have 5%, 6.6%, 10%, 13.3%, 20% and 26.6%. But these percentages are not available for all voltage ranges. You have to try to select the closest.

CTA-ID : 2053773
Was this helpful?
What can we do to improve the information ?