Technical FAQs

Ask a Question

Are the QO breakers IEC947-2 Rated?

No. For IEC ratings, order the QOXD type breakers, refer to Supplemental and Obsolescence Digest.


CTA-ID : 2053764
Was this helpful?
What can we do to improve the information ?