Technical FAQs

Ask a Question

What is the part number for an aluminum solid neutral for HCW1450-4 ?<br /><br />What solid neutral is required for an HCW1450-4 interior?

Aluminum: HCW4SN

Copper: 40517-426-51

Further I-Line neutral and ground bar information may be obtained by clicking the document link below.

Revised 4/27/04

CTA-ID : 2053721
Was this helpful?
What can we do to improve the information ?