Technical FAQs

Ask a Question

Are Power Factor Correction Capacitors available with NEMA 3R enclosures?


Issue:
Capacitors in Outdoor boxes

Product Line:
Power Factor Caps

Environment:
Fixed PFCs

Cause:
Enclosure

Resolution:
Yes. NEMA 3R power factor correction capacitors are available as a special order. Select NEMA 1 catalog numbers and add RF as a suffix, for example PFCD4006RF. From page 4-28 and 29 of Digest 175.


CTA-ID : 2053723
Was this helpful?
What can we do to improve the information ?