Technical FAQs

Ask a Question

I have an MP Masterpact breaker without terminals F1 and F2 for external power to the trip unit. Can these be added?

F1 and F2 terminals are provided only with trip units requiring power supply. This includes options: I, F, T, W, VF, C. These terminals cannot be added in the field.


CTA-ID : 2053738
Was this helpful?
What can we do to improve the information ?