Technical FAQs

Ask a Question

What is the wire range for AL800P7K lug kit for Powerpact M or P frame breaker?

Product Line:
Powerpact P frame breakers

Resolution:
Lug kit number AL800P7K will accept (2) 3/0 - 600 kcmil Al or CU wire; or 750 kcmil COMPACT Aluminum conductors.
Note that the only 750 kcmil wire this lug will accept is COMPACT aluminum.

BEWARE of manufacturer's COMPACTED aluminum wire.  It may be smaller than standard wire but it is not "COMPACT".  Southwire for example has a COMPACTED 750 kcmil AL wire with OD 1.068" that will NOT fit in this lug.
The lug OD is 0.954" and the wire must be equal to or less than that dimension to work.


CTA-ID : 2053901
Was this helpful?
What can we do to improve the information ?