Technical FAQs

Ask a Question

What is the part number for the replacement switch mechanism for a 9037HG35?

6507950251 switch mechanism. Customer must indicate class and type number of switch it`s being used on as this part number includes the cover which has the class and type numbers on it.

CTA-ID : 2053776
Was this helpful?
What can we do to improve the information ?