Technical FAQs

Ask a Question

What is the part # for the Harmony Biometric Switch demonstration bag?

XB5SBIODEMO, This includes the Biometric Switch Demo, Tower Light Demo, normal instruction sheets that come with the Biometric Push Button and the tower lights, Simplicity in One Touch - enhanced instruction sheet for the Biometric Switch, sell sheet for the Biometric Switch, sell sheet for the Tower Light that is mounted on top of the enclosure, Quick Start Guide, 120VAC-24VDC power supply, and a cloth for cleaning the touch screen window.



CTA-ID : 2053799
Was this helpful?
What can we do to improve the information ?