Technical FAQs

Ask a Question

Do the NF Nema 4/4X panelboard enclosures use the LP9618 key ?

Issue:
Do the NF Nema 4/4X panelboard enclosures use the LP9618 key  ?

Product Line:
PTFDS - FD Enclosure Systems

Environment:
Panelboard boxes sold and supported in the USA.

Cause:
Is the replacement key for the Nema 4/4X NF panelboard boxes the same as the standard panelboard key?

Resolution:
No, 80106-456-01 is the replacement key for Nema 4/4X enclosures.


















CTA-ID : 2053766
Was this helpful?
What can we do to improve the information ?