Technical FAQs

Ask a Question

Can an HVL/cc switch with fuse tripping be shipped for both direct acting trip and time delayed trip?

No. The switch will have to be shipped for direct acting fuse tripping. Later when the fuse size is increased, services will need to modify the linkage and add the time delay relay.


CTA-ID : 2053748
Was this helpful?
What can we do to improve the information ?