Technical FAQs

Ask a Question

How can Energy Connsumption (kWh) value be obtained in ATV21 drive via Modbus?

If F748 is set 0, the Power Consumption memory is cleared. If set to 1, the Power Consumption memory is retained.
The Modbus address are:
FE76 Accumulated Input Power Consumption in kWh
FE77 Accumulated Output Power Consumption in kWh


CTA-ID : 2053568
Was this helpful?
What can we do to improve the information ?