Technical FAQs

Ask a Question

Is there an alternate lug for the NSF150N breakers?

Yes. Lug 37488 which will accept one 250﾿350 kcmil Cu or AL.


CTA-ID : 2053326
Was this helpful?
What can we do to improve the information ?