Technical FAQs

Ask a Question

What is the difference between a QO1LO and an HOL1 handle lock-off accessory?

Product Line:
Circuit Breakers

Environment:
Electrical Distribution Equipment

Resolution:
The QO1LO is a clamp for holding QO single pole handle in ``ON`` or ``OFF`` position;
The HLO1 is a clamp for holding QO or Q1 either 1, 2 or 3-Pole breaker handles in ``ON`` or ``OFF`` position


CTA-ID : 2053686
Was this helpful?
What can we do to improve the information ?